Other Parts Discussed in Thread: DRV8301, CONTROLSUITE, MOTORWARE, BOOSTXL-DRV8301
Hi,
I need additional ~20A on the DRV8301 kit, i.e from 42.5 to about 60A.
I use motors of about 5-30 uH, 28VDC.
Can the power circuit handle this ?
further, for the current sense I thought of the following :
1. The full scale of the ADC for current sensing is set to 82.5A full scale, so that needs to be changed, through the resistors around the OPAMP (whose output is EXT_Ix-FB) ?
2. Rshunt - do I need to change it ? I'm thinking in sense of the drv8301... does the drv8301 uses this shunt for internal purposes or just to output the voltage on the SO0,SO1 pins ?
3. Change OC_ADJ_SET in drv8301, according to table 9 ? I actually don't understand this because the FETs being used on the board have Rdson ranging from 0.0039 to 0.0082 (and I assume all FETs have range from Rdson). This implies that the current limit is not stable at a value and the range is huge (up to more than two times between 3.9m and 8.2m). For example, the original setting for drv8301 in the software is 0.75Vds. If we calculate the current limit - this is huge - 0.75/4m = 180A !! did I get this wrong ?
Thanks a lot