Hello,
We are using TMS320F28030 Microcontroller for an Automotive Motor control application which has been to the production phase. We have implemented a function which calculates the Sum value of data stored in Flash from Address 0x3f4000 to 0x3f4100, and execute after certain interval amount of time to ensure the proper functioning of the Microcontroller Flash module.
Recently we observed that the sum value is different when we using CCS V4.2.3 when compared to CCS V5 considering the fact that the same code and debugger (TI XDS100) is used.
Could you please enlighten us on this and share the supporting document for the same.
Prompt reply will be highly appreciated.
Thanks & Regards,
Vinay Kumar