hi all,
is there is someone has worked before connected f2812 to an Ethernet controller like the microchip ones, j60 series, while both are 3.3v,
is the connection direct, and no need for pull-up resistors, am i right, or we need ones,
also, the vcc and gnd, its two different sources, its no problem,,, am i right,,,,,,
sorry but im newbie in DSP world, kindly confirm, that the only connection i need is the IN/OUT lines and the CS and CLK, so only for lines, directly connected without pull-up resistors
thanks
hasan