Hi,
I am just in the learning process of the DSP F28335. Currently I am exploring the TI library files that are needed for the initial make up of the processor such as initial clocking for every peripherals, etc. During my analysis, I found difficulty in understanding some low level of the code, which I have described below. Please help me in understanding these parts,
1) DSP2833x_CpuTimers.c
The function ConfigCpuTimer is present in this file. One of the parameters for this function is frequency. Since the CPU frequency for F28335 is 150MHz, should we give the same 150MHz as input ? Or else giving any other frequency values is possible?
Also I am not able to understand the typecasting done in the function "temp = (long) (Freq * Period)" but temp is a unsigned long value.
My roundup question: What are the maximum values, which can be given for the input parameters Freq and Period?
2) DSP2833x_usDelay.asm
- What is the maximum value for the input "LoopCount", since giving the maximum value of the data type, the function doesn't perform its intended funtionality.
Please help resolving this queries.