Other Parts Discussed in Thread: MOTORWARE, CONTROLSUITE, DRV8301, DRV8313, DRV8312
First post, I'm new. I have F28069MISO and F28069 control cards an experimenter kit "docking station". I have flashing lights but now I'd like to evaluate custom power stage hardware for control of basic motor types (3-phase variants, DC and stepper). So I'd like do the incremental build labs but I haven't found any example projects featuring incremental builds that are written for the F2806x.
I would like to stick with the F28069M hardware to take advantage of the InstaSPIN and Motion libraries when appropriate and I'm under the impression that it's better learning the newer Motorware sw implementation.
I've spent the last two days pouring over the documentation and can't decide if it's worth using the older F2803x example code as a foundation or pick apart the latest Motorware (1_01_00_12) examples. Both options are unappealing. Any suggestions? Is it worth diving into the older code? Have I missed something?
New labs due soon have been eluded to elsewhere in this form. Due they contain example projects with incremental builds for F2806x devices?
Thanks, Erich