This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Need help in selecting proper ratings BLDC Servo for TMDSHVMTRPFCKIT

Dear Community Members,

I am thinking of buying the TMDSHVMTRPFCKIT development board, to be able to control a BLDC motor rated slightly less than a kilowatt @300-400Vdc range. The BLDC motor that is being offered by TI (by Anaheim Automation) has lower ratings, so I checked out other higher rating motors from Anaheim Automation. I am pretty open to the torque ratings of the motor. I need advice on the following issues:


1. According to TMDSHVMTRPFCKIT documentation, the PFC stage is designed for 750W ratings. So I will have to bypass it, if I were to use a 1kW BLDC servo? Do I need to consider other factors in motor selection too, like peak stall current, continuous current, peak and continuous stall torque, or this board can drive any BLDC motor rated 1kW, @ <= 400Vdc rating, under rated conditions?

2. Say I decide to use the PFC and AC rectifier stage, and choose a BLDC motor with around 750 W, in 300-400 Vdc range. Will I need to consider the above listed factors, or any other special factors for that matter, before I buy the motor?

3. Finally, can fellow members who have worked with similar ratings BLDC motor, suggest to me which motor to buy in the above range of ratings (700-1000W, 300-400Vdc)?


Thank you very much for taking the time to read. Your input will be much appreciated!

Regards,

AS