This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

USING SPI LOOP BACK WITH EXTERNAL PIN CONNECTED

Hello,

We have designed a board with a F28M35H52C1 connected to an external SPI flash.

When I try to use this spi for the first time the loop back option was activated (SpiaRegs.SPICCR.bit.SPILBK = 1).

Accordind to the SPRUH22F, with this loop back option  SIMO/SOMI lines are connected internally.

Does using this option with external SPI pins connected and configured to be used as spi can dammage something ?