Other Parts Discussed in Thread: CONTROLSUITE
Dear support,
We perform properly flash m3/c28 programming on devices F28M35H52C1RFPT_YF19A5VRW G4,
DID0= 0x20400000,DID1= 0x1154804C .
Now we'get devices F28M35H52C1RFPT_YFB_39C2VKW G4,
DID0= 0x20400001,DID1= 0x11548044 .
We perform programming during Flash API library and and our programming doesn't work at all. We don't manage to erase flash sectors om M3.
Uint32 EraseSector(Uint32 uiSectorStartAddress)
{
Fapi_FlashStatusWordType oFlashStatusWord;
Log_info1("before Fapi_issueAsyncCommandWithAddress 0x%x", uiSectorStartAddress);
Fapi_StatusType oReturnCheck = Fapi_issueAsyncCommandWithAddress(Fapi_EraseSector,
(uint32 *)uiSectorStartAddress);
// Wait until FSM is done with erase sector operation
while (Fapi_checkFsmForReady() != Fapi_Status_FsmReady){}
// Verify that SectorG is erased. The Erase step itself does a verify as
// it goes. This verify is a 2nd verification that can be done.
Log_info1("before Fapi_doBlankCheck 0x%x", uiSectorStartAddress);
oReturnCheck = Fapi_doBlankCheck((uint32 *)uiSectorStartAddress,
Bzero_16KSector_u32length,
&oFlashStatusWord);
Log_info2("after Fapi_doBlankCheck 0x%x return status = 0x%x", uiSectorStartAddress, oReturnCheck);
if(oReturnCheck |= Fapi_Status_Success)
{
// Check Flash API documentation for possible errors
// If Erase command fails, use Fapi_getFsmStatus() function to get
// the FMSTAT register contents
// to see if any of the EV bit, ESUSP bit, CSTAT bit or VOLTSTAT bit is
// set (Refer to API documentation for more details)
Fapi_FlashStatusType status = Fapi_getFsmStatus();
FlashError(oReturnCheck);
}
return oReturnCheck;
}
for the sectors that we try to erase (A,B,C,D,E,F)we get Fapi_getFsmStatus = 0x11.
Sometimes i can program device in the debugger(erase succeed), but can not do it without debugger at all. I uploaded symbolTtable from device to PC and see that Fapi_getFsmStatus = 0x11 after erase of all devices.
our FlashConfiguration is the following:
void configFlashAPI(void)
{
Fapi_StatusType oReturnCheck;
Fapi_FlashBankSectorsType oFlashBankSectors;
// Disable Protection
HWREG(SYSCTL_MWRALLOW) = 0xA5A5A5A5;
// Disable Protection
DCSMUnlockZone1CSM (&Zone1KEY);
DCSMUnlockZone2CSM (&Zone2KEY);
// Gain flash pump semaphore
// This function must reside in RAM
FlashGainPump();
oReturnCheck = Fapi_initializeAPI(F021_CPU0_BASE_ADDRESS, 75);
do
{
if(oReturnCheck |= Fapi_Status_Success)
{
//Check Flash API documentation for possible errors
FlashError(oReturnCheck);
break;
}
Fapi_LibraryInfoType oLibInfo = Fapi_getLibraryInfo();
HWREG(FLASH_CONFIG_BASE + FLASHCTRL_O_FRDCNTL) = (1 << FLASHCTRL_FRDCNTL_RWAIT_S);
oReturnCheck = Fapi_setActiveFlashBank(Fapi_FlashBank0);
if(oReturnCheck |= Fapi_Status_Success)
{
FlashError(oReturnCheck);
break;
}
Fapi_DeviceInfoType info = Fapi_getDeviceInfo();
oReturnCheck = Fapi_getBankSectors(Fapi_FlashBank0,&oFlashBankSectors);
if(oReturnCheck |= Fapi_Status_Success)
{
FlashError(oReturnCheck);
break;
}
}while(0);
HWREG(FLASH_ERROR_BASE + FLASHERR_O_ECC_ENABLE) = 0x0;
Fapi_flushPipeline();
return;
}
what is the difference between two revisions that can influence on the M3 flash programming?
Could you please help us with this problem ASAP, becouse all our new devices that we'get could not be programmed.
C28 Programming work properly in both devices.
Thanks,Sabina