Is there a way to load the device-specifc gel file and the IQmath.gel file before entering Debug mode?
I am able to do it once I'm in Debug mode, but then when I exit Debug mode, I have to add IQmath.gel all over again the next time around.
I'm using: ..\..\emulation\gel\f2812.gel
If I follow this guide, CCS will only allow me to add one GEL file.
http://processors.wiki.ti.com/index.php/GSG:CCSv5.0_Adding_GEL_files_to_a_target_configuration
I am using CCS Version: 5.5.0.00077.
Thanks for your help.