Hi there,
I would like to connect my brand new Concerto Experimenter's kit F28M35H52C1 to the CCS6, but I am not having sucess.
By reading the QSG, I understood I need to solder jumpers in the R40 to R46 at the controlcard to enable using the docking JTAG. Is that correct? Besides, do I need to disable onboard JTAG?
Meanwhile, I tried to disable the docking JTAG through J8 and using the controlcard ISO JTAG. But, doing this, I had to use 2 USB connections. One for JTAG the controlcard and the other for just power supply the docking. It didn't work, so I am not able to establish a connection to the target configuration. Is it a feasible way to connect?
It was selected the XDS100v2 USB Emulator with device F28M35H52C1 as target configuration. I have the controlcard release 2.0 and Docking-Stn USB-EMU [R3].
Thank you in advance.
Douglas