HI everyone,
I cannot build the example project "enet_ptpd_m3" due to undefined MACRO constants. Concretely, the constants MAC_O_MDIX and MAC_MDIX_EN are not defined in the header file hw_ethernet.h (v202) unlike the previous version (v201). Should I manually add these constants in the v202 of the header file or use the v201 of such file.
Thanks.
Regards, Juan.