Other Parts Discussed in Thread: TMS320F2812, DAC8568EVM, DAC8568, AMC7812EVM-PDK, AMC7812
Dear All,
I am relatively inexperienced with hardware building, but have some theoretical understanding of electronics. I am trying to build a multi-channel DAC system with the following requirements:
No. DAC Channels: >=8
DAC Resolution: 12-16 bits
Settling time: 5us or less
Also, I need to play out DAC patterns for at least 200ms. i.e., assuming 16 bits resolution for DACs, I would need data memory of at least 16x8x(200ms/4us)=16x8x50k bits=800kBytes, say 1MB.
With this in mind, here is what I was hoping to do. Use a DAC8568 evm (http://www.ti.com/tool/dac8568evm) in conjunction with a TMS320F2812 eZdsp Start Kit (DSK) (http://www.ti.com/tool/tmdsezd2812). These two boards are supposed to go together through the HPA-MCU Interface Board. In the specifications of Starters kit (TMS320F2812), it is mentioned that it can address up to 1.0Mword Total external memory. I hope this can be used for the data patterns that I wish to play out on the DACs and use the onboard RAM in TMS320F2812 to store the instructions to control the DACs. Here are a few queries in this regard.
1. First, I request experienced users here to point to any pitfalls in my thinking, before I procure these components, especially on the memory front.
2. Next, would it be possible to swap a AMC7812EVM (http://www.ti.com/tool/amc7812evm-pdk) instead of DAC8568 (given their better settling times). The documentation of AMC7812EVM mentions that the board "can be connected to any modular EVM system interface card". Hence the question.
3. I would like to know of other microcontroller boards that can interface to the above DACs in a similar manner, but allow larger data storage for my DAC patterns (say from an external SD card).
I look forward to your inputs.
Regards,
Umesh Rudrapatna