This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problems getting Motor running with user.h

Other Parts Discussed in Thread: BOOSTXL-DRV8301, MOTORWARE

Dear community,

i have installed all the software and use the c2000 launchpad with BOOSTXL-DRV8301 and ccs6 to drive a 250W BLDC motor. After reading all the stuff in the Motorware package and the Information in the e2e there are some questions.

The graphical universal gui can identify the motor correct. Also the project lab2 is identifing the motor correct. (setting the bits in the globalvars to 1 to start the process) I updated in the next step my user.h to the values the gui and the lab2 generated. After restarting the system and set the "use User.h" flag to 1. The motor don't spins. There is only high current flow. If i let the software find the parameter new the motor start spinning as estimated. I have no more idea what i am doing wrong to setup my user.h correctly. Also the *.js can't be executed. I took the motor parameters from the universal gui. 

As i started the gui to use the user.h the parameters are wrong. But in the user.h the parameters are correct. Ive made the labs 1 to 3 and the user.h is ignored any time.

Can you please point me in the right direction, to setup my user.h correctly. For me in the labs are some steps missing, can anyone perhaps make a more detailed instruction to save and load the motor parameter out of the ccs-project? I want to start the motor without doing the identification every time. I know this is the lab i am doing but it doesn't work for me. 

Thank you very much 

Moritz Bente