Other Parts Discussed in Thread: DRV8312
Hi,
I have a motor with the following parameters:
L=0.39H; Rs=67ohm; kv=2.4 V/Hz
Using proj_lab03a:
The FAST Identifier returns Rs= 4753ohms.
What other parametes should I modify to get an accurate Rs?
It didn't run on the DRV8312-69M-Kit, too.
Thanks.