Hi,
I recently bought two experimenter kits F28069. One works fine but I cannot manage to connect to the second one. There seems to be some sort of driver problem. I am using the same computer, same program and the same target configuration file. The two devices should be identical.
I have noticed that when I connect the first device (the one that works fine) I have these two peripherals: TI XDS100 channel A and TI XDS100 channel B. However, when I disconnect this experimenter kit and I connect the second one, the TI XDS100 peripherals disapear and are replaced by two USB composite peripherals.
I have tried this procedure: http://e2e.ti.com/support/microcontrollers/c2000/f/171/t/21086.aspx, but the program cannot find my device so that I can reprogram it.
What can I do to make this work? I am a little disapointed that my new device is not working...
Thank you,
Myriam