Other Parts Discussed in Thread: TMS320F2812
Hello,
I am using SCI-B interface on my TMS320F2812. I am using FIFO enhancements and just receiving one character for the time being. So i have written the the program to generate an interrupt when a single character is received.
But the the problem is that the interrupt is not running for some reason and i cannot find out why. Can someone please help me.
Here is my code-
#include "DSP281x_Device.h"
#include "DSP281x_Examples.h"
#include <stdio.h>
interrupt void scibRxFifoIsr(void);
void InitSystem(void);
void Gpio_select(void);
void InitPieCtrl(void);
interrupt void scibRxFifoIsr(void);
void scib_fifo_init(void);
void Delay_1ms(long);
unsigned char rdataB; // Received data for SCI-B
void main(void)
{
// Initialize System Control:
InitSystem();
// Initalize GPIO:
Gpio_select();
//Clear all interrupts and initialize PIE vector table:
// Disable CPU interrupts
DINT;
// Initialize PIE control registers to their default state.
// The default state is all PIE interrupts disabled and flags
// are cleared.
InitPieCtrl();
// Disable CPU interrupts and clear all CPU interrupt flags:
IER = 0x0000;
IFR = 0x0000;
// Interrupts that are used in this example are re-mapped to
// ISR functions found within this file.
EALLOW;
PieVectTable.RXBINT = &scibRxFifoIsr;
EDIS;
//Initialize all the Device Peripherals:
scib_fifo_init(); // Init SCI-B
// Enable interrupts required for this example
PieCtrlRegs.PIEIER9.bit.INTx3=1; // PIE Group 9, INT3
IER = 0x100; // Enable CPU INT
EINT;
// IDLE loop. Just sit and loop forever (optional):
for(;;);
}
void InitSystem(void)
{
EALLOW;
SysCtrlRegs.WDCR= 0x0068; // Setup the watchdog
// 0x00E8 to disable the Watchdog , Prescaler = 1
// 0x00AF to NOT disable the Watchdog, Prescaler = 64
SysCtrlRegs.SCSR = 0; // Watchdog generates a RESET
SysCtrlRegs.PLLCR.bit.DIV = 10; // Setup the Clock PLL to multiply by 5
SysCtrlRegs.HISPCP.all = 0x1; // Setup Highspeed Clock Prescaler to divide by 2
SysCtrlRegs.LOSPCP.all = 0x2; // Setup Lowspeed CLock Prescaler to divide by 4
// Peripheral clock enables set for the selected peripherals.
SysCtrlRegs.PCLKCR.bit.EVAENCLK=0;
SysCtrlRegs.PCLKCR.bit.EVBENCLK=0;
SysCtrlRegs.PCLKCR.bit.SCIAENCLK=0;
SysCtrlRegs.PCLKCR.bit.SCIBENCLK=1;
SysCtrlRegs.PCLKCR.bit.MCBSPENCLK=0;
SysCtrlRegs.PCLKCR.bit.SPIENCLK=0;
SysCtrlRegs.PCLKCR.bit.ECANENCLK=0;
SysCtrlRegs.PCLKCR.bit.ADCENCLK=0;
EDIS;
}
void Gpio_select(void)
{
EALLOW;
GpioMuxRegs.GPAMUX.all = 0x0; // all GPIO port Pin's to I/O
GpioMuxRegs.GPBMUX.all = 0x0;
GpioMuxRegs.GPDMUX.all = 0x0;
GpioMuxRegs.GPFMUX.all = 0x0;
GpioMuxRegs.GPEMUX.all = 0x0;
GpioMuxRegs.GPGMUX.all = 0x0;
GpioMuxRegs.GPGMUX.bit.SCIRXDB_GPIOG5 = 1; //SCI-RX
GpioMuxRegs.GPGMUX.bit.SCITXDB_GPIOG4 = 1; //SCI-TX
GpioMuxRegs.GPADIR.all = 0x0; // GPIO PORT as input
GpioMuxRegs.GPBDIR.all = 0x00FF; // GPIO Port B15-B8 input , B7-B0 output
GpioMuxRegs.GPDDIR.all = 0x0; // GPIO PORT as input
GpioMuxRegs.GPEDIR.all = 0x0; // GPIO PORT as input
GpioMuxRegs.GPFDIR.all = 0x0; // GPIO PORT as input
GpioMuxRegs.GPGDIR.all = 0x0; // GPIO PORT as input
GpioMuxRegs.GPAQUAL.all = 0x0; // Set GPIO input qualifier values to zero
GpioMuxRegs.GPBQUAL.all = 0x0;
GpioMuxRegs.GPDQUAL.all = 0x0;
GpioMuxRegs.GPEQUAL.all = 0x0;
EDIS;
}
void InitPieCtrl(void)
{
// Disable Interrupts at the CPU level:
DINT;
// Disable the PIE
PieCtrlRegs.PIECRTL.bit.ENPIE = 0;
// Clear all PIEIER registers:
PieCtrlRegs.PIEIER1.all = 0;
PieCtrlRegs.PIEIER2.all = 0;
PieCtrlRegs.PIEIER3.all = 0;
PieCtrlRegs.PIEIER4.all = 0;
PieCtrlRegs.PIEIER5.all = 0;
PieCtrlRegs.PIEIER6.all = 0;
PieCtrlRegs.PIEIER7.all = 0;
PieCtrlRegs.PIEIER8.all = 0;
PieCtrlRegs.PIEIER9.all = 0;
PieCtrlRegs.PIEIER10.all = 0;
PieCtrlRegs.PIEIER11.all = 0;
PieCtrlRegs.PIEIER12.all = 0;
// Clear all PIEIFR registers:
PieCtrlRegs.PIEIFR1.all = 0;
PieCtrlRegs.PIEIFR2.all = 0;
PieCtrlRegs.PIEIFR3.all = 0;
PieCtrlRegs.PIEIFR4.all = 0;
PieCtrlRegs.PIEIFR5.all = 0;
PieCtrlRegs.PIEIFR6.all = 0;
PieCtrlRegs.PIEIFR7.all = 0;
PieCtrlRegs.PIEIFR8.all = 0;
PieCtrlRegs.PIEIFR9.all = 0;
PieCtrlRegs.PIEIFR10.all = 0;
PieCtrlRegs.PIEIFR11.all = 0;
PieCtrlRegs.PIEIFR12.all = 0;
}
void scib_fifo_init()
{
ScibRegs.SCICCR.all =0x0007; // 1 stop bit, No loopback
// No parity,8 char bits,
// async mode, idle-line protocol
ScibRegs.SCICTL1.all =0x0003; // enable TX, RX, internal SCICLK,
// Disable RX ERR, SLEEP, TXWAKE
ScibRegs.SCICTL2.bit.RXBKINTENA =1;
ScibRegs.SCIHBAUD =0x01;
ScibRegs.SCILBAUD =0xE7;
ScibRegs.SCICCR.bit.LOOPBKENA =1; // Enable loop back
ScibRegs.SCIFFRX.all=0x0021;
ScibRegs.SCIFFCT.all=0x00;
ScibRegs.SCICTL1.all =0x0023; // Relinquish SCI from Reset
ScibRegs.SCIFFRX.bit.RXFIFORESET=1;
}
interrupt void scibRxFifoIsr(void)
{
rdataB=ScibRegs.SCIRXBUF.all; // Read data
if(rdataB=='a')
{
GpioDataRegs.GPBDAT.all = 0x00;
Delay_1ms(1000);
}
ScibRegs.SCIFFRX.bit.RXFFOVRCLR=1; // Clear Overflow flag
ScibRegs.SCIFFRX.bit.RXFFINTCLR=1; // Clear Interrupt flag
PieCtrlRegs.PIEACK.all=0x100; // Issue PIE ack
}
void Delay_1ms(long end)
{
long i;
for (i = 0; i <(9000 * end); i++);
}
Thanks in advance.