Other Parts Discussed in Thread: TMS320F28335
Hi Team,
We are using TMS320F28335 controller in one of our product development.
We have recently observed that when the product is operated at less than -20 Degree celsius or
more than 60 degree celsius some of the controller pins are getting latched to high.
The architecture uses two DSC's(Both F28335) and
the pin that is getting latched is connected between two processors.
Problem scenario :
1) One processor has the pin as output and on the other processor this is taken as input.
2) there is a 10K resistor in between the processors.
3) When the processor for which it is output pulls the pin low, the other processor reads it as high.
It is observed that on one side of resistor the voltage is low and on the other side the voltage is high.
Queries:
1) We would like to know if there is any errata on silicon temperature range of operation
2) What is the minimum value of resistance that can be used.
3) Are latch-up issues observed with this processor earlier.
4) What are the scenarios when the pin can latch-up
Best Regards,
Viswanadham Y