Other Parts Discussed in Thread: CONTROLSUITE
Just joined the Forum and looking for some C2000 LaunchPad help with Linker Command files.
I created a simple project with CCSv6 to blink a LED (I know ... another newbie ... ) linked it with 28027_RAM_lnk.cmd and can run the application from RAM with the debugger. Life is good !!
The problem is getting the Linker to map correctly for the LaunchPad target when booting directly from Flash.
I have tried several Linker command files (including DSP2802x_Headers_nonBIOS.cmd) and none seem to work for the LaunchPad (dip SW 3 on LaunchPad set to "down" position to disable debugger). Have taken a brief look at SPRA958J - Running an Application from Internal Flash Memory and will study in more detail later.
Does anyone have a working Flash Linker Command File to use as a starting point for the C2000 Launchpad.
Would appreciate any help I can get.
Cheers, John