Other Parts Discussed in Thread: TEST2
Hi,
I designed a PCB board with TI TMS320FF28335 being a component. But I have never used DSP before, so I bought a DSP EVM to practice programming before I download the program to the DSP on the board which I designed. The problem is: the emulator works fine on the EVM board , but encounters an error when trying to connect to my board, and the error message is:
Error connecting to the target:
Error 0x00001200/-1135
Error during: OCS, Target,
Unrecoverable emulation error
The JTAG connections are the same for both boards.
can you please help me figure out the problem?
Vincent