Other Parts Discussed in Thread: CONTROLSUITE, TMS320F28335
Dear all,
My application is having the following error during compilation process:
#102 "Uint16" has already been declared in the current scope
I searched trought the code and found that it is defined to times.
First one in the "xdc/std.h":
typedef xdc_UInt16 UInt16;
Second one in the "DSP2833x_Device.h":
typedef unsigned int Uint16;
"xdc/std.h" is part of the xdctools and "DSP2833x_Device.h" is from the examples in the ControlSuite for TMS320F28335. I need to include both headers but it is not possible to compile then. I guess that it is because I'm using a newer compiler version than the used in the example. I tried several thinks like commenting the typedef in "DSP2833x_Device.h" but then the compiler says that "Uint16" is not defined.
Does someone have anys idea for solving that?
Thanks in advance,
Aitor