This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28335 Chip Not Coming out of HALT Mode

Hello.  I have a mature product that has been in the field for the last 18 months.  Just recently I have had 4 product returns where the product had gone to sleep as expected but would not wake up.  Only a full power cycle would wake the processor up.  The code to put into HALT mode is pretty simple:

// set the low power mode to HALT and execute the IDLE command

EALLOW;

if (SysCtrlRegs.PLLSTS.bit.MCLKSTS != 1) // Only enter low power mode when PLL is not in limp mode.

{

SysCtrlRegs.LPMCR0.bit.LPM = 2;

//select HALT mode

FlashRegs.FPWR.bit.PWR = 0;

//turn off Flash power during Halt Mode

AdcRegs.ADCTRL3.bit.ADCPWDN = 0;

//ditto ADC

AdcRegs.ADCTRL3.bit.ADCBGRFDN = 0;

//dittp ADC Band Gap Reference

}

EDIS;

asm(" IDLE"); /* Force device into HALT */

 

I have the interrupt configured to execute the wakeup logic.  On these defective products the wakeup executes correctly 9 out of 10 times at least.  It is not easy to to reproduce.  From our scope shots we see the crystal begin oscillating when the wakeup goes low.  On a good wakeup the crystal continues to oscillate and the DSP wakes up and the clockout shows activity.  On a bad wakeup, the crystal stops oscillating when the wakeup goes back to the high state.

 

I would appreciate any help and suggestions on this issue.  Thanks in advance.

 

Chris

  • Hi Chris,

    On these defective products the wakeup executes correctly 9 out of 10 times at least.

    Oh! This seems to be the case of Device malfunctioning. Though such an issue should not arise, but this raises a question on device genuineness.

    I'm forwarding your query to one of my TI friend who might provide you with official response.

    Regards,

    Gautam