Other Parts Discussed in Thread: CONTROLSUITE
Hello,
I just recently purchased a 28335 Experimenter Kit and I'm having some trouble seeing signals on the headers on the board. I'm running an example file that is changing the duty cycle of EPWM1. When I measure pin 23 on the experimenter board (not on the header but on the bottom of the board) I see the PWM signal. Also, I can run the same code on my peripheral explorer kit with no problems. First question is are the pins mapped one to one to the headers? Second, I started with header pin labeled 33 (the first header pin nearest the USB connector) and started measuring header pins all reference to the ground near the 3.3V 4 pin header. All of the header pins measure 3.3V. Is the dock defected? Do I need to set a jumper?