Other Parts Discussed in Thread: TMDSHVMTRINSPIN, CONTROLSUITE
I have recently purchased the TMDSHVMTRINSPIN kit to evaluate Instaspin motion. I am trying to get started with InstaSpin Motion using the GUI Composer software. After installation,it is suggested in the quick start guide that The USB Port on the Control card be connected to the PC USB. On powering the kit with the low voltage DC power supply & then connecting the cable to the USB port, I should see TIXDS100 Channel A & B appearing in the Device manager. This is not happening & hence I cannot proceed. Tried on multiple USB ports & PCs with no success.
Some Details:
High Voltage: hvmtrkit_r1p1 [Yellow PCB with black enclosure]
PN: TMDSHVMTRINSPIN
Jumper settings done as per QSG:
TMDSCNCD28069MISO
i. SW1: UP-UP
ii. SW2: DOWN-DOWN
iii. SW3: UP-UP
HVMTR_r1p1
i. Populate: J3, J4, J5, J8,
ii. Populate: M3-J5
iii. J7: Right-Middle (towards capacitors)
Any help would be appreciated since I cannot proceed.