Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

GPIO47 causes PWM problem on C28346

I have C28346 hooked up to a 3.3v source.  If gpio 47 is configured as an input, all PWM outputs work as expected and will output at 0-3.3V.  However, if gpio 47 is configured as an output, pwms 0-5 (on gpios 0-5) are outputting at 1.6-3.3V when GPIO 47 is set high. If GPIO 47 is set to output low, pwms 0-5 will output between 0-1.6V.

Any thoughts as to what may be causing this problem?  Other gpios do not seem to have this effect as gpio47.

Thanks