Hi,
I would refer to Single phase motor drive solution.
Motor specification:
-Supply voltage:140V
-Supply current:30-40A
-Sequence topology:Full-bridge
There is 3-Phase solution in the Controlsuite but not Single-Phase.
And In the following post, That is not in TI plan.
http://e2e.ti.com/support/microcontrollers/c2000/f/902/t/303716.aspx
Anyone knows Single-phase solution of C2000?
best regrds,
kyt