hello
I'm currently involved in a project aiming the development of a special motor controller.
Actually the the IC is ship with an embedded bootloader (for the M3 and C28x). But unfortunately because the bootloader of our device should work with an already define bootloader protocol and flash other satellite IC than the C28x we are not able to use the default bootloader.
So. is it possible to reuse the bootloader bank of the M3 in order to write my own bootloader or is it a true dead ROM memory ?
if the this 64K bank is available to be written how can i do that?
Siegfried van Haelst