Other Parts Discussed in Thread: F28M36P63C2
Dear e2e,
I am attempting to add code security to an F28M36 MCU project that has been working well for several months.
Basically I have a Bootloader that resides in M3 flash sector N. Flash sectors M-A are used for the Main application. The bootloader will copy a new main application from an SD Card into RAM and then burn it into Flash sectors M-A when requested.
When I change dcsm_z1_sec_values.asm to have a password other than FF... (11... for example). The bootloader continues to run, but it hangs up during the flash procedure. The has been very difficult to debug.
I have tried to use secure memory for everything to avoid problems.
My .cmd file is attached. Thank you for your help.
/*
// NOTE: IMA copied most of this file from the flash programming example project
//
//###########################################################################
// FILE: F28M36H63C2_m3.cmd
// TITLE: Linker Command File for F28M36H63C2 projects that run from FLASH
// Keep in mind that C0 and C1 are protected by the code security module.
// What this means is in most cases you will want to move to
// another memory map file which has more memory defined.
//###########################################################################
// $TI Release: F28M36x Support Library v201 $
// $Release Date: Fri Jun 7 10:37:02 CDT 2013 $
//###########################################################################
*/
//--retain=g_pfnVectors
/* The following command line options are set as part of the CCS project. */
/* If you are building using the command line, or for some reason want to */
/* define them here, you can uncomment and modify these lines as needed. */
/* If you are using CCS for building, it is probably better to make any such */
/* modifications in your CCS project and leave this file alone. */
/* */
/* --heap_size=0 */
/* --stack_size=256 */
/* --library=rtsv7M3_T_le_eabi.lib */
/* The following options allow the user to program Z1 and Z2 DCSM security */
/* values, include CSM PSWD, ECSL PSWD, GRABSECT, GRABRAM, and FLASH EXEONLY */
/* The driverlib/dcsm_z1_secvalues.s and driverlib/dcsm_z2_secvalues.s files */
/* must be included in the Flash project for the below 2 lines to take */
/* effect. */
--retain=dcsm_z1_secvalues.obj(.z1secvalues,.z1_csm_rsvd)
//--retain=dcsm_z2_secvalues.obj(.z2secvalues,.z2_csm_rsvd)
--retain=BL_REVISION.obj(.blrev)
/* System memory map */
MEMORY
{
/* Flash Block 0, Sector 0 Z1 CSM */
CSM_ECSL_Z1 : origin = 0x00200000, length = 0x0024
CSM_RSVD_Z1 : origin = 0x00200024, length = 0x000C
//CSM_RSVD_OTHER : origin = 0x00200050, length = 0x01AF //Found at TRM pg. 550, but not verified
/* Flash Block 0, Sector 0 */
RESETISR (RX) : origin = 0x00200030, length = 0x0008 /* Reset ISR is mapped to boot to Flash location */
BL_INTVECS (RX) : origin = 0x00200038, length = 0x0258
BL_FLASH (RX) : origin = 0x00200290, length = 0x7D60 // The Bootloader resides here - never touch this block (N)
BL_REVISION : origin = 0x00207FF0, length = 0x0004 //4 bytes used for the bootloader revision number
//8 empty bytes in the middle
BL_RSVD : origin = 0x00207FFC, length = 0x0004 //4 bytes reserved for resolution reduction mode
APP_RESETISR (RX) : origin = 0x00208000, length = 0x0008 // Entry point into the application
APP_INTVECS (RX) : origin = 0x00208008, length = 0x0258 // Interrupt Vectors for the application
APP_FLASH (RX) : origin = 0x00208260, length = 0xF7BA0 // The Application resides here
/* Flash Block 0, Sector 13 Z2 CSM*/
CSM_RSVD_OTHER2 : origin = 0x002FFE00, length = 0x01D0 //Note found at TRM pg. 550 (set to 0x00)
CSM_RSVD_Z2 : origin = 0x002FFFD0, length = 0x000C
CSM_ECSL_Z2 : origin = 0x002FFFDC, length = 0x0024
/* ACTUAL FLASH PAGES (KEEP FOR REFERENCE):
FLASH_N (RX) : origin = 0x00201258, length = 0x6DA8 // For storing code in Flash to copy to RAM at runtime
FLASH_M (RX) : origin = 0x00208000, length = 0x8000
FLASH_L (RX) : origin = 0x00210000, length = 0x8000
FLASH_K (RX) : origin = 0x00218000, length = 0x8000
FLASH_J (RX) : origin = 0x00220000, length = 0x20000
FLASH_I (RX) : origin = 0x00240000, length = 0x20000
FLASH_H (RX) : origin = 0x00260000, length = 0x20000
FLASH_G (RX) : origin = 0x00280000, length = 0x20000
FLASH_F (RX) : origin = 0x002A0000, length = 0x20000
FLASH_E (RX) : origin = 0x002C0000, length = 0x20000
FLASH_D (RX) : origin = 0x002E0000, length = 0x8000
FLASH_C (RX) : origin = 0x002E8000, length = 0x8000
FLASH_B (RX) : origin = 0x002F0000, length = 0x8000
FLASH_A (RX) : origin = 0x002F8000, length = 0x7FD0
*/
/* RAM */
C0 (RWX) : origin = 0x20000000, length = 0x2000
C1 (RWX) : origin = 0x20002000, length = 0x2000
BOOT_RSVD (RX) : origin = 0x20004000, length = 0x0FF8
C2 (RWX) : origin = 0x200051B0, length = 0x0E50
C3 (RWX) : origin = 0x20006000, length = 0x2000
// USED TO STORE NEW BINARY IMAGE FOR FLASHING C28
SHARED_RAM : origin = 0x20008000, length = 0x10000
/* SHARED RAM (KEEP FOR REFERENCE):
S0 (RWX) : origin = 0x20008000, length = 0x2000
S1 (RWX) : origin = 0x2000A000, length = 0x2000
S2 (RWX) : origin = 0x2000C000, length = 0x2000
S3 (RWX) : origin = 0x2000E000, length = 0x2000
S4 (RWX) : origin = 0x20010000, length = 0x2000
S5 (RWX) : origin = 0x20012000, length = 0x2000
S6 (RWX) : origin = 0x20014000, length = 0x2000
S7 (RWX) : origin = 0x20016000, length = 0x2000
*/
//USED TO STORE NEW BINARY IMAGE FOR FLASHING M3
RAM_HIGH (RWX) : origin = 0x20018000, length = 0x18000
/* ACTUAL RAM PAGES (KEEP FOR REFERENCE):
C4 (RWX) : origin = 0x20018000, length = 0x2000
C5 (RWX) : origin = 0x2001A000, length = 0x2000
C6 (RWX) : origin = 0x2001C000, length = 0x2000
C7 (RWX) : origin = 0x2001E000, length = 0x2000
C8 (RWX) : origin = 0x20020000, length = 0x2000
C9 (RWX) : origin = 0x20022000, length = 0x2000
C10 (RWX) : origin = 0x20024000, length = 0x2000
C11 (RWX) : origin = 0x20026000, length = 0x2000
C12 (RWX) : origin = 0x20028000, length = 0x2000
C13 (RWX) : origin = 0x2002A000, length = 0x2000
C14 (RWX) : origin = 0x2002C000, length = 0x2000
C15 (RWX) : origin = 0x2002E000, length = 0x2000
*/
CTOMRAM (RX) : origin = 0x2007F000, length = 0x0800
MTOCRAM (RWX) : origin = 0x2007F800, length = 0x0800
}
/* Section allocation in memory */
SECTIONS
{
.resetisr: > RESETISR
.intvecs: > BL_INTVECS
.text : > BL_FLASH
.const : > BL_FLASH
.cinit : > BL_FLASH
.pinit : > BL_FLASH
.vtable : > C0
.data : > C0
.bss : > C1
.sysmem : > C0
.stack : > C0
.z1secvalues : > CSM_ECSL_Z1
.z1_csm_rsvd : > CSM_RSVD_Z1
// .z2secvalues : > CSM_ECSL_Z2
// .z2_csm_rsvd : > CSM_RSVD_Z2
.blrev : > BL_REVISION
m3rambuffer : >> RAM_HIGH
c28rambuffer : >> SHARED_RAM
GROUP
{
ramfuncs
{
-l F021_API_CortexM3_LE.lib
}
} LOAD = BL_FLASH,
RUN = C0,
LOAD_START(RamfuncsLoadStart),
LOAD_SIZE(RamfuncsLoadSize),
LOAD_END(RamfuncsLoadEnd),
RUN_START(RamfuncsRunStart),
RUN_SIZE(RamfuncsRunSize),
RUN_END(RamfuncsRunEnd),
PAGE = 0
GROUP : > MTOCRAM
{
PUTBUFFER
PUTWRITEIDX
GETREADIDX
}
GROUP : > CTOMRAM
{
GETBUFFER : TYPE = DSECT
GETWRITEIDX : TYPE = DSECT
PUTREADIDX : TYPE = DSECT
}
}
__STACK_TOP = __stack + 256;
Isaac