Other Parts Discussed in Thread: CONTROLSUITE
Hi
I am using F28377xD . I would like to know if the below given steps are right for setting up my usb interface on the card , as I am still waiting for the USB female to mini wire and am a bit confused with the process required to be done .
1) Put all the J1- J7 jumpers on pins 1 and 2.
2) Turn on Switch Position 2 on A:SW1 .
3) Connect USB with a hex file to the microcontroller card and run usb_dev_bulk_cpu01 and the program would convert from lower to upper case and vice versa ?
I do not have the mentioned file 'usb_bulk_example' or a tools directory to know if this is required. Will I need this ?
Kind Regards