Other Parts Discussed in Thread: TMS320F2801, TMS320F2808
Hey everybody,
I am using microcontroller TMS320F2801 in welding inverter. It communicates with front panel through CAN interface.
Some processors communicate well, some just sometimes. They are not able to receive mailbox or two (or 5).
Changing processor to TMS320F2808 (which should be possible) brings more problems. No 2808 communicates properly, but each in different way. Some doesn't receive mailbox 1, some mailbox 5, etc. Looks like it's depend on ID number.
Hardware and software is the same in all devices. CAN module setting keeps the way described in users manual (but now I am not sure with anything).
Does someone have an idea whats wrong?
Thanks,
Tomas.