Other Parts Discussed in Thread: AFE032
Hallo,
I still working with the TMDSPLCKIT V3 and have implemented a G3 Application on CENELEC frequency band.
The next step is to implement the same application in a higher frequency range to get higher data rates. I saw the the TMDSPLCKIT V3 can be used with a F28M35 controller card and a discrete AFE. Do I have to implement this discrete AFE by my self or is a board available?
As alternative I saw the TMDSPLCKITV4-ARIB with the AFE032 but in the release notes of the G3- FW-Package V6020 is still written:
-HW Platform: F28M35X + Discrete AFE
CQ001249: AFE032 is not working after running for a while
Is on the TMDSPLCKITV4-ARIB a discrete and the AFE032 implemented? Or is the FW working with the AFE032?
I look forward to hearing from you very soon
Best Regards