Other Parts Discussed in Thread: CONTROLSUITE
Hi,
Has anyone interfaced a F28xxx processor with the ADC121c021 using I2C ?
If there are code snippets available ?
I would appreciate receiving any example.
Thank You
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: CONTROLSUITE
Hi,
Has anyone interfaced a F28xxx processor with the ADC121c021 using I2C ?
If there are code snippets available ?
I would appreciate receiving any example.
Thank You
Hi qcsoft,
If there are code snippets available ?I would appreciate receiving any example.
No such example file exist, you'll have to work on your own. Yes, if any difficulty faced while implementing : this forum's there to help you out.
BTW which controller in C2000 series are you planning to use? These mcus have enough ADC channels to play with then why an external one?
Regards,
Gautam
Is there any similar I2C interfaces to an ADC documents ?
Code for external ADC interface using I2C or respective doc is not available as I previously mentioned. controlSuite has a sample code for EEPROM interface and for documentation on I2C you can refer peripheral documentation.
Regards,
Gautam