Other Parts Discussed in Thread: CONTROLSUITE
HI
I am trying to communicate between two F28069 control sticks using SPI. I have gone through the spi_loopback examples in control suite and considering it as base,i changed the SPICCR.4 = 0 to disable it and SPICTL.2=1/0 for master/slave mode.
The connections between two control sticks is as:
Pin24 i.e. Gpio16(master) to pin 24 i.e Gpio 16(slave) ..... SPISIMOA
Pin20 i.e. Gpio17(master) to pin 20 i.e Gpio 17(slave) ..... SPISOMIA
Pin29 i.e. Gpio18(master) to pin 29 i.e Gpio 18(slave) ..... SPICLKA
Pin25 i.e. Gpio19(master) to pin 25 i.e Gpio 19(slave) ..... SPISISTEA
Please help ,as i m stuck with this for last two days....
thanks