Other Parts Discussed in Thread: TMS320F28335, CONTROLSUITE
We're looking to setup SCI-A on a TMS320F28335 eZdsp board as a transmit-only non-periodic messaging system for diagnostic and coverage data as pulling large amount of data over the debugger/USB connection is very slow (5-10 minutes for 20kb text file).
We've followed through the SCI Echoback example contained in the controlsuite and tried to set up the initial configuration to match that; however, the data transmitted out once it has been placed into the SCITXBUF is garbage/corrupted on the terminal screen.
The current initialization sequence is as follows:
InitializeSys()
{
InitializePLL(0xA, 0x2);
SysCtrlRegs.PCLKCR0.bit.SCIAENCLK = 1;
InitializeInterrupts();
InitializePieVectors();
InitializeFlash();
GpioCtrlRegs.GPADIR.bit.GPIO29 = 1;
GpioCtrlRegs.GPAPUD.bit.GPIO29 = 0;
GpioCtrlRegs.GPAMUX2.bit.BPIO29 = 1;
InitializeADC();
InitializeI2C();
InitializeSPI();
InitializeMcBSP();
InitializePWM();
InitializeTimers();
SciaRegs.SCIFFTX.all = 0xE040;
SciaRegs.SCIFFRX.all = 0x204F;
SciaRegs.SCIFFCT.all = 0x0;
SciaRegs.SCICCR.all = 0x7;
SciaRegs.SCICTL1.all = 0x2;
SciaRegs.SCICTL2.all = 0x1;
SciaRegs.SCIHBAUD = 0x1;
SciaRegs.SCILBAUD = 0x44;
SciaRegs.SCICTL1.all = 0x22;
}
void scia_xmit(char a)
{
while (SciaRegs.SCIFFTX.bit.TXFFST != 0) {}
SciaRegs.SCITXBUF = a;
}
void scia_msg(char *msg)
{
int i = 0;
while (msg[i] != '\0')
{
scia_xmit(msg[i]);
i++;
}
}
int main(void)
{
InitializeSys();
scia_msg("Hello World!\r\n");
}
On the PC side, I have an instance of PuTTY running with 9600 baud, 8 data bits, 1 stop bit, no parity, no flow control.
The data I receive is garbled/corrupted and unreadable.
As part of the initialization, we are making use of external ram (ZONE7; ZONE6 is unused, so we could swap to that if necessary) - is it possible that is causing the issue?
We're using the default baud rate from the Echoback example (9600) for a 20 Mhz clock, which I believe is what we're setup as via the PLL. Trying to try other rates did not appear to make a difference. Attempting to use the BRR for a 37.5 Mhz clock didn't make a different either (just in case...).
Any assistance would be greatly appreciated.