This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Powerline Communication System based on TMS320C2000 F28335 TMDSPLCKIT-v2

Hi there, 

I'm working on a communication project with F28335. I'm building a power line communication system and need to transmit data continuously from my PC to the board, then to the other board and finally received by the other PC. 

I've used the echoback example in the control Suite for the SCI transmission and another example of physical layer transimission over the power line. 8322.ti_plc_prime_phy_example.rar 

Do you have any suggestion for this project? How can I combine these two examples together to build a system?

Thank you. Any help is greatly appreciated.

Qiaozi