Other Parts Discussed in Thread: TMDSCNCDH52C1
I have a project using an older TMDXCNCDH52C1 card which is fine. I've just bought some more cards. The original part no is discontinued; these are TMDSCNCDH52C1 (note subtly different part number), which look identical but clearly aren't. Code Composer was reluctant to connect to the device, and when it did I can't program the flash.
Cortex_M3_0: GEL Output: Memory Map Initialization Complete
Cortex_M3_0: Error connecting to the target: (Error -1141 @ 0x0) Device is not responding to the request. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 5.0.569.0)
Cortex_M3_0: Error connecting to the target: (Error -1141 @ 0x0) Device is not responding to the request. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 5.0.569.0)
Cortex_M3_0: Error connecting to the target: (Error -1266 @ 0x0) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 5.0.569.0)
Cortex_M3_0: GEL Output: Watchdog Timers Enabled
Cortex_M3_0: GEL Output: UARTs Enabled
Cortex_M3_0: Loader: One or more sections of your program falls into a memory region that is not writable. These regions will not actually be written to the target. Check your linker configuration and/or memory map.
Cortex_M3_0: File Loader: Data verification failed at address 0x00200030 Please verify target memory and memory map.
Cortex_M3_0: Unable to terminate memory download: (Error -1003 @ 0x2BC5) Internal error: Invalid parameter passed to function. Restart the application. If error persists, please report the error. (Emulation package 5.0.569.0)
Cortex_M3_0: GEL: File: D:\_Work\Workspace_CCS\temperatureController_M3\Flash\temperatureController_m3.out: a data verification error occurred, file load failed.
It's not a faulty board; a second one behaves identically. Substituting an original ControlCARD works first time reliably.
Does anyone know what might have changed to cause this problem?
Thanks,
Roy Gwinn