Other Parts Discussed in Thread: CONTROLSUITE
Hi,
I want to configure uart in an example project for my F2837xD eval. board. Does uartstdio.h/.c files in /utils have to used? How can I include in the project.
Thanks
Prakash
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: CONTROLSUITE
Hi,
I want to configure uart in an example project for my F2837xD eval. board. Does uartstdio.h/.c files in /utils have to used? How can I include in the project.
Thanks
Prakash
Hi Prakash,
Prakash Patel said:I want to configure uart in an example project for my F2837xD eval. board. Does uartstdio.h/.c files in /utils have to used? How can I include in the project.
You can find a ready-made example code named sci_echoback (uart) and so on in controlSuite.
C:\ti\controlSUITE\device_support\F2837xD\v110\F2837xD_examples_Cpu1\sci_echoback
Regards,
Gautam
Thanks Gautam for the reply.
I have one more question. Can I use this code for serial communication because I am using A:J1 USB/UART connector for connecting with PC. Do I need to add USB interface in order for it to work ?
Your help is greatly appreciated.
Regards
Prakash
Prakash Patel said:Can I use this code for serial communication because I am using A:J1 USB/UART connector for connecting with PC. Do I need to add USB interface in order for it to work ?
Yes, why not! No, you might not need the USB interface (If you're able to power the board externally). Just check the schematic whether you need a level converter or is it present. Usually SCIA can be directly connected to serial port but do check the schematic.
Regards,
Gautam
Prakash Patel said:It is working with the hardware.
That's Great, Prakash!
Goodluck & Regards,
Gautam