This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PM_Sensor less project using F28069

Other Parts Discussed in Thread: CONTROLSUITE, TMDSCNCD28069ISO

Hi Chris,

I am working on  C:\ti\controlSUITE\development_kits\DRV8312-C2-KIT_v128\PM_Sensorless  project using  drv8312-69m-kit. I think  “PM_Sensorless” project can be implemented on drv8312-69m-kit which is based F28069 controller .

 

Want  to do incremental build  as explained in “Sensorless FOC of PMSM” reference document located at C:\ti\controlSUITE\development_kits\DRV8312-C2-KIT_v128\PM_Sensorless\~Docs

 

  1. Imported the project in to CCS5
  2. I could build  and run the project .

 

Here are my questions

 

  1. Using Real time mode,   I  can see “BackTicker”  variable continuously refreshing  . But as explained in the “Sensorless FOC of PMSM” reference document, don’t find “IsrTicker” Variable is not increasing , what could be the reason  this variable is not changing?
  2. Is my project running as it supposed and all the settings on the board as needed ?
  3. I am also not able to create the Graphs of Ta,Tb and Tc ??
  4. What other changes are needed to implement “PM_Sensorless” project on F28069 controller ?

 

I also want to cross check , upon right click selected configuration as  F28069x_RAM[Active] , is this correct selection ?

 

 

Thanks for your help.

RK