Other Parts Discussed in Thread: TMS320F28335
Dear all,
I've got a problem with mailboxes while using the eCANA peripheral of the TMS320F28335. I've configured mailbox 0 to 7 for reception and 8 to 12 for transmission. In this way the program works well but if I try to configure in addition one of the mailboxes between 16 and 31 for transmission, my application only sends the message that has the mailbox between the 16 and 31.
My first guess was that it could be a problem with the CAN mode but I've checked it and the register is (CANMC.13 = 1).
Does anyone have an idea of what else could it be?
Thanks in advance,
Aitor