Other Parts Discussed in Thread: DRV8301, UNIFLASH, MOTORWARE, CONTROLSUITE
Hello everyone,
at first my setup:
Hardware: Own Hardware (similar to LAUNCHXL-F28027 with BOOSTXL-DRV8301) and a custom BLDC motor
IDE: Code Composer Studio 6.0.0.00190 and GUI Composer 1.0.0.201308252300 (rcp-main)
Software: LAB10A
So here is my problem:
We developed an own hardware board. It is designed like the schematics for launchpad and boostxl_drv8301, should really be a 1:1 copy of it. We can program the controller and test connections with code composer studio and uniflash are perfectly working. But the software is somehow not starting.
After a few days of investigation we found out, that the watchdog is repeatedly triggered. The XRS also shows that. The timing is perfect and matches the predefined watchdog value. So the software seems to try to start but then the watchdog resets the controller. It's just LAB10A, the exact same software running on a launchpad is working.
Is there anything else than the out file we have to program? I think I remember that I read something about preflashed math routines on the launchpad, is that correct and do we have to program them on our own?
I thank you in advance and hope for an answer soon!
BR,
Patrick