Other Parts Discussed in Thread: AMC1204, ADS1204, ADS1209
Hi
I have specified SM320F2808 device to be used for audio processing with real time data stream of 40K sample per second (audio signal range is 1Khz and 3.5Khz) where it would be demodulated into binary pattern (audio telemetry). The DSP role is to de-noise and de-echo signal. I already have bandpass filter (2 pole each side)
Is SM320F2808 right device for this application, would DSP have sufficient capacity to process audio signal in real time?
I'm looking for 16 bit ADC suitable for this job (125C grade is a must), will SPI cope with fast data rate, where can I find driver for this task?
Analogue Device make top notch quality ADC with SPORT bus, how to make SM320F2808 work on ADC via SPORT bus, has anyone have driver or c code for that?
Thanks