Other Parts Discussed in Thread: TMS320F28055
I am using TMS320F28055.
for simple code, I made it without fifo.
is it possible to run ?
void write_section(void)
{
Uint16 i2c_i = 0;
i2c_status = I2caRegs.I2CSTR.all;
if(I2caRegs.I2CSTR.bit.BB == 1)
{
return ;
}
I2caRegs.I2CSAR = I2C_SLAVE_ADDR;
I2caRegs.I2CCNT = 130; //Set count to 1 characters plus 1 address bytes
I2caRegs.I2CMDR.bit.IRS = 1; // Reliquish I2C from reset
I2caRegs.I2CMDR.bit.TRX = 1; //Set to Transmit mode
I2caRegs.I2CMDR.bit.MST = 1; //Set to Master mode
I2caRegs.I2CMDR.bit.FREE = 1; //Run in FREE mode
I2caRegs.I2CMDR.bit.STT = 1; //Send the start bit, transmission will follow
I2caRegs.I2CDXR = high_addr; //Send camera high address
I2caRegs.I2CDXR = low_addr;
for(i2c_i = 0 ; i2c_i < 128 ; i2c_i++)
{
I2caRegs.I2CDXR = sand_read_buffer[i2c_i];
}
I2caRegs.I2CMDR.bit.STP = 1; //Stop when internal counter becomes 0
while (I2caRegs.I2CSTR.bit.XRDY != 1) {}// Wait until Tx buffer is empty again
DELAY_US(10);
}
do i have to ues interrupt and fifo to run i2c? or are there any method without fifo and interrupt?