Hello!
I bought a "C2000 Power Line Modem Developer's Kit (TMDSPLCKIT-V3". After I finished the installation procedure, I found the "APPENDIX E – PHY Example Project for F28069" chapter in the "TI PLC Development Kit User Guide (Version 0.92)". However, it is not possible for me to load/compile the example project, because I do not have the "ti_g3_phy_example.zip" file (where all the source code is available).
I also downloaded a newer version -> G3_SDK_Package_V7316 but there is no file named like this too. I installed all files in the recommended directories and I'm searching for the file in this location: C:\Texas Instruments\G3DevelopmentEvalPackageV6010\F2806x\SW.
However, in the PRIME directory (PRIME_DDK_PackageV7910) everything seems allright, because here are CC project files.
Can I download the G3 Example files from somewhere?
I appreciate your help,
regards
Lukas