I use 4 EEPROMs of microchip 24LC1025 in 28335 i2c bus.
I use i2c tx & rx fifo interrupt (max 16 byte). the 24LC1025 memory is manged by page unit (of 128 byte size).
When I write into eeprom, all operation is ACKED.
I have a problem, which is the ACK Polling procedure.
ACK polling procedure is only that a write control byte for check ACKED.
How can I send only a write control byte?
the followings are my code part.:
// ---------------- Sending
I2caRegs.I2CSAR = pMsg->slaveAddress;
I2caRegs.I2CMDR.all = 0x6EA0; // (RM=1, no FIFO data)
//---------------- In ISR i2c_int1a_Isr
if(IntSource ==I2C_ARDY_ISRC)
{
// OK. Acked.
// end of it.
}
if( IntSource == I2C_NACK_ISRC )
{
if( I2caRegs.I2CSTR.bit.NACK == 1)
{
I2caRegs.I2CMDR.bit.STP = 1;
I2caRegs.I2CSTR.all = I2C_CLR_NACK_BIT;
// NACKed.
// re-try ACK polling
}
}
//------------------- end of code -----------------------------
Cho, Cheol-Hyeon.