This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EzDSP28335 I/O Pins

Using the EzDSP28335 board.  Any suggestions on which of the 88 GPIO pins should not be configured becuase they may affect operation of the external Ram, boot from flask e.t.c.

Not using external memory in my design.

 

  • Hi Otu,

    Otu Eno said:
    Using the EzDSP28335 board.  Any suggestions on which of the 88 GPIO pins should not be configured becuase they may affect operation of the external Ram, boot from flask e.t.c.

    Simply refer the schematics of the board and you'll get the whole idea. Esp. JTAG pins should be avoided even though they can be used as GPIOs.

    Regards,

    Gautam