Other Parts Discussed in Thread: MOTORWARE
Hello,
I am using DRV8312-69M-KIT
My system is using motor from http://www.iflight-rc.com/product/iPower-Brushless-Motor-iPower-GBM-Series-iPower-Gimbal-Brushless-Motor-GBM4008-150T.html
It has Magnetic Quadrature encoder AS5047D attached externally.
I have run the lab 2a/2b/5c successfully for Motor Identification
I am trying to run lab12a but the motor does not even move and it is holding the position firmly.
also My Motor winding are getting Hot if gMotorVars.Flag_Run_Identify” equal to 1
I have check the polarity of A/B/I correctly. I have even check the output from encoder using scope to make sure that encoder is giving out signals.
What might be the possible reason that sensorless project work fine and with sensored system the motor is not moving at all.
Tushar