Other Parts Discussed in Thread: MOTORWARE, DRV8312
Hello everybody,
We have prototype electric car and want to change our inverter control to InstaSPIN. This produces some questions, as the hardware already exists and we have to look for ways how it can fit into the InstaSPIN-environment.
The first problem is, that in control of electric cars, sensorless algorithms are not common, because they are not considered safe and reliable enough. Our motor (PM, ca. 10 kW) has a built-in hall-sensor (60 degree-signals), and we would like to use this sensor. As far as I have read in the User-Guide, only incremental encoders are supported.
Now we have some alternatives:
- Implement our own algorithm for startup and switch then to InstaSPIN-FOC, and use the Hall-Signals to supervise InstaSPIN's angle estimation
- Directly use InstaSPIN's algorithms (also for startup) and only use the Hall-Signals for supervision
- Not use InstaSPIN for this application
What would you recommend us to do?
Would it be possible to use InstaSPIN BLDC for startup, and then switch to FOC? Or is this a good idea? It should be possible to use InstaSPIN BLDC with a Hall-Sensor, right?
Is the InstaSPIN-Startup-procedure still only an open-loop-algorithm, or is there a closed-loop (signal injection) method in the newest version?
Thanks for your answers!
Philipp