Other Parts Discussed in Thread: BOOSTXL-DRV8301, DRV8301
I have added a BoostXL-DRV8301 as a second parallel motor drive to the DRV8301-LS31-KIT. So I am trying to control two motors with one set of PWM signals from the MCU. The regular motor output of the DRV8301-LS31-KIT connected to the supplied Teknic M2310 motor and works fine.
Jumper wires are attached to the J5 connector to the BoostXL board. Attachment is as follows:
| DRV8301 | PIN | BoostXL |
| J5-6 | EN_GATE | J4-15 |
| J5-9 | FAULTn | J3-6 |
| J5-12 | OCTWh | J3-8 |
| J5-13 | DC_CAL | J4-17 |
| J5-22 | PWM_CL | J4-12 |
| J5-23 | PWM_AL | J4-4 |
| J5-24 | PWM_AL | J4-8 |
| J5-25 | PWM_AL | J4-2 |
| J5-26 | PWM_CH | J4-10 |
| J5-28 | PWM_BH | J4-6 |
| J5-39 | GND | J3-3 |
| J5-40 | GND | J4-1 |
As can be seen, all the outputs of the MCU to the DRV8301 are connected but not all the return signals fromt he DRV8301 to the MCU. I am basing the sensorless measurements from one motor.
Please identify what signals must be connected for operation and which ones don't have to be.
Thanks
Alan