I am using the TMDSHVMTRPFCKIT with the HVACI Sensorless project. I am on build level 3, which attempts to verify the dq-axis current regulation.
It says:
§ Check pi_id.Fdb in the watch windows with continuous refresh feature whether or not it should be keeping track pi_id.Ref for PI module. If not, adjust its PI gains properly.
§ Check pi_iq.Fdb in the watch windows with continuous refresh feature whether or not it should be keeping track pi_iq.Ref for PI module. If not, adjust its PI gains properly.
It works within certain velocity, when I adjust the SpeedRef above 0.5 (Q24) the pi_idFdb and pi_iqFdb are not keeping track the pi_idRef and pi_iq.Ref respectively.
I’ve tried to adjust the PI gains without success. What could I try ?
Thanks in advance !