Other Parts Discussed in Thread: TMS320F28055
I am using TMS320F28055 on my designed board, and XDS-200 J-TAG Emulator.
SCI-A and SCI-B are open to PC. in the case of SCI-A, it connects with RS-232. another is connected with FTDI(USB to Uart)
the problem shows channel B(SCI-B)
after downloading the program, I sand hex code to TMS320F28055 via SCI-B(GPIO22, GPIO23)
C28xx: Error: (Error -1135 @ 0x93C2) The emulator reported an error. Confirm emulator configuration and connections, reset the emulator, and retry the operation. (Emulation package 5.0.872.0)
C28xx: Trouble Halting Target CPU: (Error -1044 @ 0x0) The emulator reported an error. Confirm emulator configuration and connections, reset the emulator, and retry the operation. (Emulation package 5.0.872.0)
this kind of error appears. and cannot work SCI-B.
GPIO22 and GPIO23 are not connected with JTAG PIN,
I do not know the reason. because both are not totally related
Could you give me some advice?