Other Parts Discussed in Thread: TMS320F28069F
Dear all,
I am using TMS320F28069F controller and motorware13 example implementation in my custom board for AC induction motor 415V/50Hz system. My motor data are 415V, 50Hz, 2900Rpm, 13.3Amp, 2Pole, 7.5kW and motor taking 3.9Amps in no load condition (no load on shaft).
I face below two problem.
-
When motor running in 10Hz, it will take 3.9Amps and motor running Ok, but when I set 1.00Hz, motor running in force angle and it's current increasing up to 13.3Amps. I cant understand why this happen?
-
If I set 10.0hz(600rpm) Ref frequency, Acceleration time is 2Sec and I enable gMotorVars.Flag_Run_Identify = 1 than output frequency can not smoothly accelerate. It will take some jerk in starting. I think In starting Output frequency uncontrolled and after that it will controlled.
Is any one know about this type issue?